STM32F0xx BxCAN Loop-back Transfer Delay
Hi,
I am working on STM32F042.
I have setup the BxCAN peripheral into loop-back silent mode, and it works fine. I can transfer and receive every single frame I am transmitting and no error conditions are detected.
However, I have noticed that when I want to transmit a frame, there is a delay of about 37 ms (!) between setting the TXRQ (request to transmit) bit and the call to the CAN interrupt handler once the flag RQCP (transmission completed) is set.
Has anyone experienced similar delays? Is this happening only in loopback mode?
Thank you,
Marco