Exit from STOP mode
Hi everyone,
I'm slightly confused here.
I'm putting my micro into stop mode, but I can't seem to wake it up using an interrupt.
Here's how I'm setting it:
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_NVIC_ClearPendingIRQ(EXTI4_IRQn);
HAL_NVIC_SetPriority(EXTI4_IRQn, 0, 1);
HAL_NVIC_ClearPendingIRQ(EXTI4_IRQn);
HAL_NVIC_EnableIRQ(EXTI4_IRQn);
HAL_SuspendTick();
//Enter STOP mode (deepsleep) and set the exit condition as wait-for-interrupt
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
// HSI clock is selected after wakeup from deepsleep, reset clock to HSE and reset clock tree.
SystemClock_Config();
HAL_ResumeTick();Prior to entering stop mode, I set the pin that I want to trigger the interrupt on. then I suspend the systick and enter the stop mode with WFI activated.
After this, if I trigger GPIOA - PIN4, nothing happens. If I don't enter stop mode, then the interrupt operates normaly, that is it'll enter the interrupt handler. After exiting stop mode, I reset the clock tree using systemclock_config. But at this point, I can't seem to exit stop mode.
Does anyone know what I could be doing wrong ?
Thanks in advance for any help