Skip to main content
James Murray
Associate III
December 10, 2018
Solved

STM32F746 Cortex-M7 silicon bug. Singlestep lands in interrupt handler

  • December 10, 2018
  • 19 replies
  • 6963 views

I'm running into the Cortex M7 r0p0, r0p1 bug where single-stepping is impossible due to the processor handling an interrupt instead.

i.e.

http://www.keil.com/support/docs/3778.htm

I'm using OpenOCD and it is reporting:

Warn : Silicon bug: single stepping will enter pending exception handler!

As per title, this is with an STM32F746Z on a Nucleo 144 which has the bug. STM32F769N worked as expected.

Are there any plans from ST to release a fixed ARM core in the 746 or 745?

regards

James

This topic has been closed for replies.
Best answer by Tesla DeLorean

>>Are there any plans from ST to release a fixed ARM core in the 746 or 745?

This topic has been discussed before, and no, they don't plan on updating the core. The debugging case is a ppm/ppb use case, and doesn't impact product level functionality.

The F722 has a newer core, as do the F76x/77x and H7 parts.

19 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
December 10, 2018

>>Are there any plans from ST to release a fixed ARM core in the 746 or 745?

This topic has been discussed before, and no, they don't plan on updating the core. The debugging case is a ppm/ppb use case, and doesn't impact product level functionality.

The F722 has a newer core, as do the F76x/77x and H7 parts.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
James Murray
Associate III
October 18, 2020

Just to clarify, do you mean F76x/77x or F7x6/7x7 ?

The latter is more in line with the product page: https://www.st.com/en/microcontrollers-microprocessors/stm32f7-series.html (Which I find illogical, the sub-family number would make a lot more sense as the middle number not the final one.)

e.g. F746, F756, F767, F777

James

James Murray
Associate III
December 10, 2018

Thanks for the answer, I did try searching, but perhaps not hard enough.

Shame that the chip won't be fixed as it currently makes debugging very difficult.

James

Tesla DeLorean
Guru
December 10, 2018
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
December 20, 2018

SEGGER have implemented a workaround for this hardware core bug in their J-Link debuggers. On-board ST-LINK can be converted to J-Link OB.

https://www.segger.com/products/debug-probes/j-link/models/other-j-links/st-link-on-board/

Mario Ghecea
Associate II
October 16, 2020

It does not work in Segger J-Link OB either...Seems once again ST Sold a $70 dollar board without single stepping ability so shifting blame to Segger is a poor implementation of a joke without re-spinning the Silicone...It only works by using the ST Link Utiliy in a special tweaked mode...Open OCD does not work using ST Link or upgrading to Segger. It cannot step as specified above...Single Stepping fails completely in Segger J-Link OB by jumping steps because it cannot stop on a breakpoint and runs hay-wire...Same deal with ST-Link...Sad as it looked like a promising board! Unfortunately it is Junk in any debug mode and I have tried them all...0693W000004JyjtQAC.jpg0693W000004JyhiQAC.jpg

Tesla DeLorean
Guru
October 16, 2020

It is an ARM issue, which they resolved in subsequent spins of their deliverable IP. ST was one of the first companies to get ARM CM7 silicon for them to work with.

ST isn't going to do-over the chip layout and validation, the design team(s) rotated into the next products, it is out of the design cycle, and into the fab/production cycle, and it will be there until end-of-life. Its not a process of constant introspection and correction of a design that's already left the factory.

If you really need to single step your code to understand flow/dynamics then you'll need to pick a part which is a close proxy or use more classical analysis methods.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
James Murray
Associate III
October 18, 2020

I have a workaround that allows me to use breakpoints on STM32F745 with the on-board STlink and OpenOCD.

When you hit the breakpoint:

Step

(lands in an interrupt)

Set Registers -> primask to 1

Run (seems like it didn't do anything)

Step

Continue stepping like normal.

But it is indeed a PITA.

James

Piranha
Principal III
March 6, 2021

@James Murray​ , @Mario Ghecea​ 

Guys, the workaround by SEGGER actually works out of the box. I'm using it in EmBitz through J-Link GDB Server with no special configuration and no issues. If it doesn't work, it's probably because of something else. Just a blind guess - OpenOCD.

Mario Ghecea
Associate II
March 11, 2021

Stop lying and more able people than you have been trying to deceive this thread and this is a known fact that that entire line from ARM had a fault in it probably by design...So save us the BS...What you work for Elon Musk with the fake vids of rockets landing backwards ? Seriously save us the time wasted reading your messages....People here have nested interrupt complex issues not 1+2+3 = (code your wrote)