Skip to main content
MAqee
Associate
December 7, 2018
Question

Why do leds of STM32F407VG not glow when it is connected to external power source(5V,1A)?

Hi

I am currently working on stm32f407vg discovery board. I have written code for stm32f407vg in Atollic True studio. But when i connect stm32f407vg discovery board to external source (power bank), built in leds (orange(LD3),green(LD4),red(LD5),blue(LD6)) of stm32f407vg do not glow but when i connect to PC they glow. Also when external power source is connected to stm32f407vg, LD1 of stm32f407vg blinks red but when it is connected to PC it (LD1) glows continuously with colors of red and green. Please guide me. how can i fix this issue?

Thanks in advance.

    This topic has been closed for replies.

    3 replies

    saiteja
    Associate III
    December 7, 2018

    what is input voltage you are getting to led when you connected with external power source

    MAqee
    MAqeeAuthor
    Associate
    December 10, 2018

    I have given 5V form a power bank to the both pins (5v on the P2) in section 6.2 and (VDD on the P1) at page 25 in a user manual UM1472 that both pins can be used as power supply.

    Here user manual is attached.

    Tesla DeLorean
    Guru
    December 10, 2018

    Surely VDD should be 3V

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..