Skip to main content
Glebiys
Associate
December 6, 2018
Question

Choosing a reliable DC / DC converter to power the controller (12V / 5V)

  • December 6, 2018
  • 0 replies
  • 553 views

Hi!

I design a board on which there will be several microcontrollers (STM32 and ATMEGA328), 12V comes on the board and I need to lower this voltage to 5V. In addition to the controllers, I will power a few more sensors and LEDs.

I am trying to find a reliable dc / dc converter. Sample requirements:

- Input voltage: 12V

- Output voltage: 5V

- Output current 2.5-3A

- High efficiency

- Resistance to noise

- Minimum strapping

After reading the recommendations, I saw a DC / DC converter ST1S40.

The question is whether this converter is suitable for powering my board? Are there any other options?

This topic has been closed for replies.