Skip to main content
cionu
Visitor II
December 3, 2018
Question

How i can migrate from F4/L1 to L4?

Hi. I want to connect a STM32L475RG board with an shield,

(S2868A1) which comunicated on SPI protocol. More that, i want to connect these 2 components with another Stm32L4 and S2868a1, via S2-LP mode.

Can somebody offer me a code or explain how i can migrate from F4/L1 to L4?

This topic has been closed for replies.

4 replies

ST Technical Moderator
December 4, 2018

Hello,

You can start with X-CUBE-SUBG1 expansion software package to start developing using S2-LP and S2868A1 expansion boards.

There are these application notes available regarding the migration from STM32F4 and STM32L1 to STM32L4 that can help you on the migration.

  • AN4616 Application note Migrating from STM32F401 and STM32F411 lines to STM32L4 Series and STM32L4+ Series microcontrollers

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/87/fc/79/9d/3c/cc/49/84/DM00144612/files/DM00144612.pdf/jcr:content/translations/en.DM00144612.pdf

  • AN4821 Application note Migrating from STM32F405/415 line and STM32F407/417 line to STM32L4 Series and STM32L4+ Series microcontrollers

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/02/46/be/cf/31/75/4e/de/DM00263732/files/DM00263732.pdf/jcr:content/translations/en.DM00263732.pdf

  • AN4612 Application note Migrating from STM32L1 Series to STM32L4 Series and STM32L4+ Series microcontrollers

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/4b/2a/a4/df/99/31/49/71/DM00141025/files/DM00141025.pdf/jcr:content/translations/en.DM00141025.pdf

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
December 4, 2018

Porting is one of those staples of embedded development.

Find a like-for-like type platform moving from one NUCLEO to another typically involves less pin changes. The F4 and L4 have some architectural differences.

Make a scratch or donor project on the target board, get USART, SWV an basic functionality working. Mod the code in a way that simplifies the reception of the original code.

Use a good merge tool. Pull in code a section at a time. The code doesn't have to execute, at some level you are trying to insure the project continues to build, and address syntax errors/changes in the API, or pin usage. How much you bring in at a time depends on how overwhelming the changes are.

I migrated the LoRa code to L4 and F7 platform via NUCLEO boards, I also went from NUCLEO-64 to NUCLEO-144 within the same families, this allowed changes in pin/USART usage to be understood, addressed and refactored within a platform that was still buildable. For the NUCLEO in a given platform it was then an easier port to DISCO or custom boards.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LCout
Visitor II
January 29, 2019

Hello,

Have you managed to connect your two STM32L4 ?

I have the same issue, your help would be very great !

waclawek.jan
Super User
January 29, 2019

Start a new thread stating what's exactly your problem.

JW