Skip to main content
Barbie
Associate III
December 3, 2018
Question

Is SafeRTOS support in STM32CUBEMX?

  • December 3, 2018
  • 1 reply
  • 807 views

If I want to use the SafeRTOS for critical issue can I use it in the cubeMX as I use today the FreeRTOS?

If it is possible or not at this stage, and if yes what adaptation do I need to do to use it?

Is there any guide for immigrate Safe RTOS to CUBEMX?

Regards

Bar.

    This topic has been closed for replies.

    1 reply

    AvaTar
    Senior III
    December 3, 2018

    I'd say no.

    SafeRTOS is a pre-certified product by Wittenstein, and not freeware.

    Licence costs use to be in the 5/6 digit figure range.

    > Is there any guide for immigrate Safe RTOS to CUBEMX?

    Probably possible, but sounds to me like implanting a Rolls-Royce engine into a golf buggy.