Skip to main content
SPraj.15
Associate II
December 2, 2018
Question

3-wire SPI Configuration

  • December 2, 2018
  • 2 replies
  • 1274 views

Hello,

Currently i'm working on STM30F030 controller.

I want to connect TFT display with this controller, display has three pin for SPI (SDA,SCL & CS) and used only for write operation.

so how to configure controller for 3-wire SPI

If i have to connect MOSI(controller) pin with SDA(display)and left MISO pin as it is, it is ok ?

any problem occur during communication if MISO is floating ?

Thank you

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    December 2, 2018

    There's no problem with not using MISO. You don't even need to assign a pin to MISO in the GPIO AF matrix.

    JW

    Senior
    March 11, 2024

    Hi @SPraj.15 

    this is an old thread, but I´m still curious if you made the 3-wire SPI working?

    I`m struggling with it already for days...