Skip to main content
SChav
Associate
Nov 30, 2018 4:42 AM UTC
Question

Unable to transmit data when B-L072z powered with batteries

I want to power my B-L072Z (all in one LoRa module) with battery. i am able to power the board but not able to transmit/receive data. What should I do. Tell me any solution asap.

Thank you.

Regrd,

Sagar

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    Nov 30, 2018 5:08 AM UTC

    >> What should I do.

    Instrument the code, output diagnostic via a UART, and figure out what's happening.

    The boards work with batteries, work out what you're doing wrong.

    https://community.st.com/s/question/0D50X0000A1mniaSQA/not-able-to-send-packets-with-battery-powered-for-bl072cz

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    SChav
    SChavAuthor
    Associate
    Nov 30, 2018 5:36 AM UTC

    Thank you@Clive.

    But I am not doing any extra thing. I just burned the Sample code (Given by semtech). Packets are transmitted successfully If I power the board with USB cable(Through PC).

    But it doesn't work if I remove the USB power and insert the Batteries as a input power source.

    Please help me out.

    Regrd,

    Sagar

    sergug
    Visitor II
    Dec 7, 2018 10:22 AM UTC

    Solution:

    From UM2115 User manual "Discovery kit for LoRaWAN™ and LPWAN protocols with STM32L0": 

    "If the board is supplied by CN13, by battery or by CN11, SB37 must be removed to release the RESET pin managed by ST-LINK. In that case the ST-LINK is no more powered."