Hi, I am using STM32F407ZGT6 with mikroe 1369 ( https://www.mikroe.com/mikromedia-4-stm32f4 ) I need to capture falling edge of external signal and read the time its took from starting the function till falling edge detected.
- November 27, 2018
- 7 replies
- 1965 views
Hi, I am using STM32F407ZGT6 with mikroe 1369 ( https://www.mikroe.com/mikromedia-4-stm32f4 )
I need to capture falling edge of external signal and read the time its took from starting the function till falling edge detected.
I read maual but some how i am not getting right and its not working properly, i am getting 28 and 30 mS time regardless of signal present or not. Can some one guide me please and tell me what is wrong with this my code.
void InitTimer3(){
// GPIO Input: TIME alternate function for CH1,PA6
GPIO_Alternate_Function_Enable(&_GPIO_MODULE_TIM3_CH1_PA6);
GPIO_Set_Pin_Mode(&GPIOA_BASE,_GPIO_PIN_6,_GPIO_CFG_MODE_INPUT);
//disableInterrupts(); // disable global interrupts
RCC_APB1ENR.TIM3EN = 1;
RCC_AHB1ENR |= 0x1 ; //clock enable to GPIOA
TIM3_CR1.CEN = 0;
TIM3_PSC = 1;
TIM3_ARR = 37499;
TIM3_CCER.CC1E=1;
TIM3_CCER.CC1P = 0;
TIM3_CCER.CC1NP = 1; // Falling edage
TIM3_CCMR1_Input =1; // INPUT CAPTURE CH1
TIM3_CCR1 =1; //page 641
NVIC_IntEnable(IVT_INT_TIM3);
TIM3_DIER.TIE = 1; // enable interupt
TIM3_DIER.CC1IE = 1;
TIM3_DIER.UIE = 1;
TIM3_CR1.CEN = 1;
TIM3_EGR.UG = 1; // Reinit the counter
TIM3_EGR = 1;
enableInterrupts();
}
int EdgeCounter = 0;
void Timer3_interrupt() iv IVT_INT_TIM3 {
TIM3_SR.UIF = 0; // reset counter
LED_B=1;
LED_G=0;
LED_R=0;
// if falling edage detected
if(TIM3_SR.CC1IF== 1)//falling edage detect
{
TIM3_CR1.CEN = 0; // timer off
Rly_D=0;
disableInterrupts(); // disable global interrupts
//TIM3_SRbits.CC1IF == 0; // clear flag
// Displya timer code here
LED_B=0;
LED_G=0;
LED_R=1;
}
}
void EL_TimeB() {
InitTimer3();
delay_ms(1000);
EnableInterrupts();
NVIC_IntEnable(IVT_INT_TIM3);
delay_ms(1000);
Rly_D=1;
while(( TIM3_SRbits.CC1IF == 0 ) || (EdgeCounter< 5000 )) {
NVIC_IntEnable(IVT_INT_TIM3);
EdgeCounter++;
}
LED_B=1;
LED_G=1;
LED_R=0;
j = TIM3_CNT; // copy counter
TIM3_CNT = 0; // reset counter
TIM3_EGR.UG = 1; // update TIM3 registers
TIM3_SRbits.CC1IF = 0 ; // Clear flag
strcpy(ELTIME_main.Caption," " );
DrawLabel(&ELTIME_main);
LongWordToStr(j, text3);
strcpy(ELTIME_main.Caption,text3 );
ELTIME_main.Font_Color = Cl_green;
DrawLabel(&ELTIME_main);
}