Skip to main content
mboua
Associate
November 23, 2018
Question

STM32F411VE ADC interrupt not working

  • November 23, 2018
  • 0 replies
  • 448 views

My code works fine without interrupt (I tried polling the ADC value) but when I enabled the interrupt, it didn't work - while debugging in Keil, it never reaches the 

ADC_IRQHandler()

, Also I found that the EOC flag is always set(in the while loop)

This is my code:

#include "stm32f4xx.h" // Device header

volatile int16_t k=0;

int main()

{

RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN | RCC_AHB1ENR_GPIOAEN ;

RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;

GPIOA->MODER |= GPIO_MODER_MODE0; //analog input

GPIOA->PUPDR &=~ GPIO_PUPDR_PUPD0;

GPIOD->MODER |= GPIO_MODER_MODE13_0;//ouput

GPIOD->MODER &=~ GPIO_MODER_MODE13_1;

GPIOD->OTYPER &=~ GPIO_OTYPER_OT13;

GPIOD->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR13_0 ;

GPIOD->PUPDR &=~ GPIO_PUPDR_PUPD13 ;

GPIOD->ODR &=~ GPIO_ODR_OD13;

ADC1->CR2 |= ADC_CR2_ADON | ADC_CR2_CONT;

ADC1->SMPR2 |= ADC_SMPR2_SMP0_1;

ADC1->SQR3 &=~ ADC_SQR3_SQ1_4; //CHANNEL 0 (PA0)

ADC1->CR1 |= ADC_CR1_EOCIE;

NVIC_EnableIRQ(ADC_IRQn);

NVIC_SetPriority(ADC_IRQn,0);

ADC1->CR2 |= ADC_CR2_SWSTART;

while(1)

{

}

}

void ADC_IRQHandler()

{

k= ADC1->DR;

if(k>2000)

{

GPIOD->ODR ^= GPIO_ODR_OD13;

}

}

    This topic has been closed for replies.