Skip to main content
RTous
Visitor II
November 21, 2018
Solved

What are the difference among operating modes in magnetometer of LIS3mdl in terms of the number of samples used to generate each output sample?

  • November 21, 2018
  • 1 reply
  • 762 views

What are the difference among operating modes in magnetometer of LIS3mdl in terms of the number of samples used to generate each output sample?

For example, I found that in ISM303DAC the number of samples used to generate

output sample is four times less in Low-Power mode than the number used in

High-Resolution mode. As you know the operation modes in ISM303DAC and IIS2MDC are just two modes including low power and high resolution, but in LIS3MDL there are 4 different modes of LP, MP, HP and UHP. 

So,,

1- please let me know these difference in terms of number of samples per data output. 

2- In addition I want to know if there is any difference in resolution of operating modes? For example if I select the Low power mode in LIS3mdl with +-2Gauss range, how would be the resolution in other modes?

    This topic has been closed for replies.
    Best answer by Miroslav BATEK

    We do not share number of samples used for averaging, but we provide information about the RMS noise in different modes.

    0690X000006CVJbQAO.png

    The resolution is the same for all modes.

    1 reply

    Miroslav BATEKBest answer
    ST Employee
    November 28, 2018

    We do not share number of samples used for averaging, but we provide information about the RMS noise in different modes.

    0690X000006CVJbQAO.png

    The resolution is the same for all modes.