Skip to main content
DBara.11
Associate II
November 21, 2018
Question

How can I rewrite peripheral block? My MCU is STM32F103VCT6?

  • November 21, 2018
  • 4 replies
  • 990 views

Hi, community!

I had a problem, when chip burned out in my device, I bought new. I installed it in the main board and programmed Flash Memory. All passed success, a device works, but there are some bugs. I assume that the peripheral devices are incorrectly configured. But I don't succeed to program the peripheral block of memory, that is start address - 0x4000 0000 and ends address - 0x5fff FFFF. I tried to program each section of the block separately, starting at address 0x4000 0000, with size 0x3ff .For example, on the block of RTC, ST Link Utility shows an error: Programming error @: 0x40002804. I have firmware for each section with size 0x3FF. What can it be with constrained? How can I program periphery? Thanks in advance.

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    November 21, 2018

    They aren't memory cells, in many cases the values written can't be read back, ie USART->DR you write a transmit register, you read back a receiver register, and USART->SR reports internal status of the USART, not anything you wrote in.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    DBara.11
    DBara.11Author
    Associate II
    November 21, 2018

    Thanks great, I got it. So, have I any ways to configure the peripherals using by ST Link utility and ST-Link/V2 programmer? I'm beginner, and I have a little experience. 

    Tesla DeLorean
    Guru
    November 21, 2018

    >>I'm beginner, and I have a little experience. 

    Ok, so WHY are you doing this? What purpose does it serve?

    The ST-LINK is capable of peeking and poking memory within the device, the debugger would do this to probe peripherals, etc. but it's not how you typically program the device. Usually you write your own code to set up the peripherals, and download and execute that code on the target.

    You could turn off verification?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..