Keil uVision + ST HAL Drivers + ST USB CDC Middleware port to GNU GCC
Dear all,
I am on the process of switching to GNU GCC for compiling an already working project. Most of the functionality has been tested. There is a failing test though: The USB VCP drivers do not seem to perform good.
The client side (PC-Windows) is tested and working using Overlapped serial port (tests performed with loopback achieve max. throughout without hiccups).
The board code was developed using Keil uVision and compiled using ARM compiler V6.9 (also tested at max. throughout without problems). Now, I switched to GNU Tools ARM Embedded v7.0 compiler. Tried disabling all optimizations but still the same failure: after several (random) packets sent from client to board, the client is unable to send any single char more to the board. The board is still able to send packets, but the debugger shows no sign of receive (and the client serial handler is also timing out).
I cannot think of any piece of code that might be useful but, should anyone be keen on looking into it, I would gladly share it.
Thank you very much for your time.
Best regards,
Xavi