Skip to main content
Dmitri
Associate II
November 20, 2018
Question

Error downloading FW.F1.1.7.0 MCU package

  • November 20, 2018
  • 12 replies
  • 3392 views

Hi,

recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:

In the log I see:

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:919 - Problem, file not found on Server

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:491 - Problem, file not found on Server : stm32cube_fw_f1_v170.zip.

Is v1.7.0 package available to download?

thanks,

Dmitri

This topic has been closed for replies.

12 replies

Tesla DeLorean
Guru
November 20, 2018

ST looks to have got a bit ahead of themselves, issue from here also, expect it to be resolved shortly. ​ @Khouloud GARSI​ 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee
November 21, 2018

Hi @Dmitri​ ,

Issue confirmed from our side and highlighted internally.

Sorry for this inconvenience. This will be fixed ASAP!

Khouloud.

Houda GHABRI
ST Employee
November 21, 2018

Hello @Dmitri​ 

Thanks for your feedback.

FW F1 1.7.0 will be available Tomorrow after doing a refresh in update Manager.

Sorry for the inconvenience.

Best regards,

Houda

Khouloud GARSI
ST Employee
November 21, 2018

Hi @Dmitri​ ,

Issue solved: The STM32F1 v1.7.0 is now available for download.

Khouloud.

Tesla DeLorean
Guru
November 21, 2018

Confirmed, have it mirrored if anyone needs it, or the other releases. The F7.1.13.0 was 1.2GB!!

ST should really consider hosting torrents for those on lower bandwidth connections, download limits or those who have intermittent connections which might benefit from a restartable download, ie continue rather than start over...

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
fm_it
Associate
November 23, 2018

Still having this problem. Can you provide a mirror? Thanks

LOVEKUSH PRATAP
Associate II
December 21, 2018

I'm still getting this error

error downloading the following files: stm32cube_fw_f1_v170.zip(cannot unzip) stm32cubemx

Tesla DeLorean
Guru
December 21, 2018

Well the .ZIP should be in the Repository, you can Check/Test it with something like WinRAR.

More critically the system will fail this way if your hard drive is out of space. Figure you're going to need more than 3.6 GB free to download and unpack

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..