Skip to main content
damien_lobb
Associate III
November 14, 2018
Question

SD Card on the IDW04A1

  • November 14, 2018
  • 1 reply
  • 694 views

Hi,

I am using the IDW04A1 WiFi module for a project where I want to transfer potentially large files to a server. Is there a way of accessing the SD slot from my MCU?

I am using the STM32F401RE MCU and currently I use an external SD to save files. If I can access the on board SD card slot that would make things a lot simpler.

Thanks

This topic has been closed for replies.

1 reply

Elio Cometti
Visitor II
November 19, 2018

​Hi,

you several way to transfer files from/to the SD card:

  • through the command interface, using filesystem commands (AT+S.FSC/FSP/...)
  • through the air by TFTP or HTTP commands

The SD card is also accessible through the on board http(s) server.

Does this answer your question?

Regards,

Elio