Skip to main content
NRAME
Visitor II
November 12, 2018
Question

STM8S001J3M3 ------- pb4 pin is not accessing

  • November 12, 2018
  • 0 replies
  • 949 views

Hello,

I am trying to access all the 5 gpio pins out of FIVE Gpio pins I am accessing 4 gpio pinss i.e (PD6/PA1 ,PA3,PC5,PC6).

------->Port d and port c are accessing normally but port b is not able to access.

------->As per data sheet if we use swim pin as gpio we should use 5 sec delay in the main function .but is not working.

#define PB_ODR     *(unsigned char*)0x5005

#define PB_DDR     *(unsigned char*)0x5007

#define PB_CR1     *(unsigned char*)0x5008

#define PB_IDR     *(unsigned char*)0x5006    

//#define WWDG_CR  *(unsigned char*)0x50D1

unsigned long int dl;

int i;

void main()

{

   for(dl = 0; dl < 500000; dl++);//delay for 5sec

   PB_ODR = 0x00; // Turn all pins of port B to low

   PB_DDR |= 1 << 4; // 0x00100000 PB4is now output

   PB_CR1 |= 1 << 4; // 0x00100000 PB4 is now pushpull

   while(1)        {

    (dl = 0; dl < 500000; dl++);

     PB_ODR |= 1 << 4; //led on

     for (dl = 0; dl < 500000; dl++);

       PB_ODR &= ~(1 << 4); //led off

       }

}

THIS IS NOT WORKING,PLEASE HELP ME.

THANKS IN ADVANCE.

    This topic has been closed for replies.