How can I use STM32 F030R8 as i2c slave using interrupt?
Since quite some time I am trying to find a way for an STM32 chip to receive and send data as a slave over i2c. The master always sends the same amount of bytes and after sending these bytes, requests two bytes back from the slave. I used the CubeMX example software for i2c with succes, however this example code as found here:
This code works and enabling a 'global i2c interrupt' and triggering an LED in this interrupt works as well. However when I try to put the code in the interrupt, the LED does not even go on. The LED is just for testing and in the end I would like to be able to receive information through i2c on an interrupt.
Putting following code in the main works for one receive and one send, however i would like to replace this code to the interrupt, which does not work as is:
if(HAL_I2C_Slave_Receive_DMA(&hi2c2, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK)
{
// Transfer error in reception process
Error_Handler();
}
while (HAL_I2C_GetState(&hi2c2) != HAL_I2C_STATE_READY)
{
}
if(HAL_I2C_Slave_Transmit_DMA(&hi2c2, (uint8_t*)aRxBuffer, 2)!= HAL_OK)
{
// Transfer error in transmission process
Error_Handler();
}
the function initializing the i2c is as follows:
static void MX_I2C2_Init(void)
{
hi2c2.Instance = I2C2;
hi2c2.Init.Timing = 0x20303E5D;
hi2c2.Init.OwnAddress1 = I2C_ADDRESS;
hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c2.Init.OwnAddress2 = 0;
hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
In CubeMX there is an NVIC enabled for DMA and i2c. Anybody who can help me out?
Help is very much appreciated.