How to building a custom external loader for a custom board based on a STM32F4 MCU?
Hi, community:
I'm working on a custom board based on a STM32F7 MCU,which I have use the MCU is STM32F750Z8T6 and spi flash is W25Q064AJVSSIQT(Winbond).
But the assets (images, font ...) are too large to be loaded into the memory of the MCU and have to be loaded directly into the external flash.
For this issue I need the external loader which will allow the STM32 ST-LINK Utility & STM32CubeProgrammer to load the code into the external flash.
In order to the STM32 ST-LINK Utility & STM32CubeProgrammer can load the code into the external flash.
I have find the example: "N25Q512A_STM32F769I-EVAL external loader example", that I was to try modify and then it working fine.
At the same time, I'm working on another custom board based on a STM32F4 MCU with the framework, this custom board I have use the MCU is the STM32F446ZET6 and spi flash is W25Q064AJVSSIQT(Winbond).
So, I also need the external loader which will allow the STM32 ST-LINK Utility & STM32CubeProgrammer to load the code into the external flash.
But, I can't find any external loader example let me to modify for STM32H series or STM32F series or STM32L series MCU, because I am using these series MCU.
Thanks in advance.