Skip to main content
BRick
Visitor II
November 1, 2018
Question

How to start the RTC in the STM32F2xx?

  • November 1, 2018
  • 2 replies
  • 697 views

How to start the RTC (real time clock) in the STM32F2xx processor with a 25 Mhz OSC

This topic has been closed for replies.

2 replies

ST Technical Moderator
November 1, 2018

Hello,

You can start with RTC example within STM32CubeF2 firmware package and modify this working application depending on your needs:

STM32Cube_FW_F2_V1.7.0\Projects\STM32F207ZG-Nucleo\Examples\RTC

You can also use STM32CubeMX tool, this allow you to choose the microcontroller, select the peripherals you want and map them to pins graphically. Then, build and generate your starting project with initialization C code.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
November 1, 2018

You want to clock it off the 25 MHz source (ie divided down HSE), or do you plan on using a 32.768 KHz LSE crystal?

I don't think the former would permit the device going into STANDBY, etc, but it would hold good time.

Should be able divide the 25 MHz to 1 MHz or less required by the RTC, and then prescaled and divided some more.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..