Skip to main content
Khoo.B
Associate III
October 24, 2018
Question

Is it possible to configure the IWDG timer to 30 minutes?

  • October 24, 2018
  • 5 replies
  • 1347 views

I have an IoT hardware (using STM32L152) that carry out some tasks and go to STOP mode for 30 minutes. Then, it will wake up and repeat the same process again.

Now, I would like to add the watchdog timer to ensure everything works fine. My question is - can we set the countdown timer to 30 minutes? I have seen on other discussion that it is not possible to configure the watchdog timer to such a long period.

Any suggestions? Thank you very much!

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    October 24, 2018

    I think you'll find the counter and prescaler are too small.

    Think you have to use RTC Alarm(s)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Jeroen3
    Senior
    October 24, 2018

    @Community member​ is right. Maximum 28 seconds.

    Khoo.B
    Khoo.BAuthor
    Associate III
    October 24, 2018

    Ok, thanks for the suggestion. Would it be possible to turn it off?

    I have seen in other discussions that an alternative work around is to wake up from the STOP mode every <28 seconds to reset the counter. Would this have a significant impact to the power consumption?

    AvaTar
    Senior III
    October 24, 2018

    An once activated watchdog timer cannot be turned off.

    For an application with 30 minutes sleep times, I would not consider a watchdog.

    Khoo.B
    Khoo.BAuthor
    Associate III
    October 24, 2018

    What would you recommend in this case? An external watch dog?