Skip to main content
khuan.81
Associate
October 21, 2018
Question

STM32F446RE I2S can't output clock

hi all,

I wan to use PA4, PA5 and PA7 as I2S.

but can't output clk. follow is code for I2S setting:

// clock setting

  RCC_PLLI2SConfig(16, 334, 2, 7, 7);

  RCC_I2SCLKConfig(RCC_I2SBus_APB1, RCC_I2SCLKSource_PLLI2S);

  //RCC_I2SCLKConfig(RCC_I2SBus_APB2, RCC_I2SCLKSource_PLLI2S);

  RCC_PLLI2SCmd(ENABLE);

  while(RCC_GetFlagStatus(RCC_FLAG_PLLI2SRDY) == RESET);

u8 I2S1_GPIO_Init(void)

{

  u8 res;

  GPIO_InitTypeDef GPIO_InitStructure;

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;//

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;//

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz;//

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;//

  GPIO_Init(GPIOA, &GPIO_InitStructure);//

   

  GPIO_PinAFConfig(GPIOA,GPIO_PinSource4,GPIO_AF_SPI1); //

  GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_SPI1); //

  GPIO_PinAFConfig(GPIOA,GPIO_PinSource7,GPIO_AF_SPI1); //

return 0;

}

void I2S1_Init(u16 I2S_Standard, u16 I2S_Mode, u16 I2S_Clock_Polarity, u16 I2S_DataFormat)

{

  I2S_InitTypeDef I2S_InitStructure;

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_SPI1, ENABLE); 

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_SPI1, DISABLE); 

  I2S_InitStructure.I2S_Mode = I2S_Mode;

  I2S_InitStructure.I2S_Standard = I2S_Standard;

  I2S_InitStructure.I2S_DataFormat = I2S_DataFormat; 

  I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Disable; 

  I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_Default; 

  I2S_InitStructure.I2S_CPOL = I2S_Clock_Polarity; 

  I2S_Init(SPI1, &I2S_InitStructure); /

  SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Rx, ENABLE); 

  I2S_Cmd(SPI1, ENABLE); 

}

...

void main(void)

{

  I2S1_GPIO_Init();

I2S1_Init(I2S_Standard_Phillips,I2S_Mode_MasterRx,I2S_CPOL_Low,I2S_DataFormat_16b);

  while (1)

  {

    asm("nop");

  }

}

    This topic has been closed for replies.

    6 replies

    waclawek.jan
    Super User
    October 21, 2018

    Read out and check/post the content of relevant GPIO and SPI/I2S registers.

    JW

    khuan.81
    khuan.81Author
    Associate
    October 24, 2018

    I have check all the pin. and change the RCC setting. but all can't work. can you help me. or have some demo share to me.

    Thanks

    Kenny

    waclawek.jan
    Super User
    October 24, 2018

    As I've said, read out and check or post the content of relevant GPIO and SPI/I2S registers.

    JW

    waclawek.jan
    Super User
    October 24, 2018

    As I've said, read out and check or post the content of relevant GPIO and SPI/I2S registers.

    JW

    waclawek.jan
    Super User
    October 24, 2018

    [doubled post due to forum bug]

    waclawek.jan
    Super User
    October 24, 2018

    [doubled post due to forum bug]