Visitor II
October 18, 2018
Question
STM32F030F4 MCU and STMStudio
- October 18, 2018
- 0 replies
- 504 views
STM32F030F4 MCU. I import the variables, I want to see, in the STMStudio. Imported well. But the value of the variable is always displayed zero. Does this MCU support STMStudio? I have: ST-Link/V2 original. SWD protocol.
If the MCU is supported, then what could be the reason?
The variable count varies from 0 to 8. The result working of the program I is visible on the oscilloscope. But in the STMStudio, the variable count is always zero.
Thank!