Skip to main content
Apill
Associate III
October 16, 2018
Solved

continous conversion of ADC and storing the data in memory card

  • October 16, 2018
  • 4 replies
  • 1034 views

Hi,

I am trying to store the converted data from ADC to memory card. as of now i can able to store the data and read the values of adc but when i tried to store the values of adc in memory card i could not able to do. i have used the below code.

I have mounted and declared objects related to sd card(FATFS) globally.

By using the below code i could only able to save the last value of adc but i would like to store every value of adc that has been converted since beginning to end ( till i stop).

I presumed as i have declared adc in interrupt mode after every conversion of adc it comes to the below function9cnvcpltcallback) so i have added lines related to sd card. right now, i would like to konw how can i continously store the values of adc pin in sd card.

Please let me know.

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)

{

 /* Prevent unused argument(s) compilation warning */

 UNUSED(hadc);

unsigned int temp=0; 

adcval= HAL_ADC_GetValue(&hadc1);

 /* NOTE : This function Should not be modified, when the callback is needed,

      the HAL_ADC_ConvCpltCallback could be implemented in the user file

  */

temp = adcval; 

f_open(&myFILE, "Write1.TXT\0", FA_WRITE | FA_CREATE_ALWAYS);

f_printf(&myFILE, "%d\r\n",temp);

f_close(&myFILE); 

}

-

Thanks,

Ashok

This topic has been closed for replies.
Best answer by AvaTar

Using a text format, i.e. a literal number strings instead of binaries, will make the evaluation much easier.

If you are concerned about throughput, don't write each value individually, rather collect and write blocks.

FATFS access in an interrupt context will break your application.

4 replies

AvaTar
AvaTarBest answer
Senior III
October 17, 2018

Using a text format, i.e. a literal number strings instead of binaries, will make the evaluation much easier.

If you are concerned about throughput, don't write each value individually, rather collect and write blocks.

FATFS access in an interrupt context will break your application.

Tesla DeLorean
Guru
October 17, 2018

For speed and efficiency you'd want to write 16 KB or 32 KB blocks.​ Do it in a foreground task.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Apill
ApillAuthor
Associate III
October 22, 2018

@Community member​  you mean i shouldnt use interrupts interfacing with FATFS ? could you please elaborate your last sentence.

AvaTar
Senior III
October 23, 2018

No, I mean you should call lengthy code like FATF calls from within interrupts.

This will block other interrupts, or follow-ups.

A SD card is an opaque unit. If a simple write happens to involve a block erase, it could take several milliseconds.