Skip to main content
Manikandan K
Associate III
October 16, 2018
Question

Interrupt problem

  • October 16, 2018
  • 2 replies
  • 704 views

Without Interrupt signal STM32F207 print continuously.How to avoid it...

void EXTI9_5_IRQHandler(void)

{

 /* USER CODE BEGIN EXTI9_5_IRQn 0 */

 /* USER CODE END EXTI9_5_IRQn 0 */

   printf("\n\rInterrupt Occur\n\r");

 /* USER CODE BEGIN EXTI9_5_IRQn 1 */

 /* USER CODE END EXTI9_5_IRQn 1 */

}

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    October 16, 2018

    >> print continuously.How to avoid it...

    Try clearing the interrupt source...

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Manikandan K
    Associate III
    October 16, 2018

    void EXTI9_5_IRQHandler(void)

    {

     /* USER CODE BEGIN EXTI9_5_IRQn 0 */

     /* USER CODE END EXTI9_5_IRQn 0 */

     HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_6);

     /* USER CODE BEGIN EXTI9_5_IRQn 1 */

     /* USER CODE END EXTI9_5_IRQn 1 */

    }

    ==========================================================================

    void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)

    {

     /* EXTI line interrupt detected */

     if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)

     {

       __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);

       HAL_GPIO_EXTI_Callback(GPIO_Pin);

     }

    }

    ===========================================================================

    void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {

       if (GPIO_Pin == INTERRUPT_Pin) {

          printf("\n\rInterrupt Occur\n\r");

       }

    }

    When I use this code ,and I just placed the jumper in interrupt pin, the Interrupt get occur without any input signal.Even though I set low priority