Question
How to integrate the parameters setup in MC workbench with IAR workbench for STEVAL-ESC001V1?
I am able to generate a IAR workbench workspace from MC workbench after setting all the parameters but I am stuck.I am generating a 490Hz PWM signal with 50% duty cycle but the motor doesn't rotate.Is it possible to change the PWM frequency in MC workbench? Am I making some other mistake?