Skip to main content
JDecl
Visitor II
October 15, 2018
Question

USBMSD not working on STEVAL-STLCS01V1

  • October 15, 2018
  • 1 reply
  • 685 views

Hi,

I am currently working with a STEVAL-STLCS01V1 (SensorTile) board for a project. One of the functionalities that I have to implement is the possibility to use the module as a Mass Storage Device (with an SD card). While CDC works fine, MSD does not. Although the SensorTile does show up among the USB devices in the system overview on my MacBook, It does not show up as a removable drive, meaning I cannot read the data stored on the SD card.

​

After debugging I found that the "Init" and "GetCapacity" functions in the "usbd_storage.c" work like they should. In the "read" function, blocks of 512Byte are read, like expected, but unfortunately the device does not show up as a removable drive.

Would there be an example project for the SensorTile ​available somewhere? This could probably help me find the problem in my code.

Best regards,

Jaimy

​

    This topic has been closed for replies.

    1 reply

    dbgarasiya
    Senior
    December 14, 2019

    you just have to configure sd card well & make some changes in usb_storage file it will show drive automatically

    you don't have to change anything in main file .

    Best of luck