Skip to main content
David Ledger
Associate III
October 15, 2018
Question

USB ESD Protection -> USBLC6-2

  • October 15, 2018
  • 0 replies
  • 1026 views

Hello,

I couldn't find a better category for this.

I'm using the USBLC6-2 for USB protection in a product that could potentially have a 20 V USB line (USB-PD). Like this:

0690X000006CBRDQA4.png

However, the VDD line would be clamped by this IC, is it acceptable to drop the VDD line like this and separately clamp it:

0690X000006CBRIQA4.png

The internal diagram for the protection IC is as follows:

 0690X000006CBRNQA4.png

The pin on the left is the I/O pin. The USB data line is not clamped to the power rail, it seems to clamp through the zener but I'm concerned that there is some black box functionality in this device.

This topic has been closed for replies.