cancel
Showing results for 
Search instead for 
Did you mean: 

What is Radc for STM32H743?

Singh.Harjit
Senior II

DS12110 Rev 5, notes for Figure 40. says it should be in Table 85 but it isn't. Rain and Cadc are in the Table 85.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
PTowl
Associate

Hello all,

Would also like to know the answer to this one.

Anyone any idea??

Regards,

CHead
Associate III

I suspect it may differ for fast versus slow channels. I would also like to know.

CHead
Associate III

I got a reply from ST in a support ticket. Their recommendation is to use table 185 in the datasheet (it’s in the revision V section, but the rep said it applies to revision Y as well).

Singh.Harjit
Senior II

​The Rev 6 datasheet still calls out Radc in two places and says look for it in two tables. This note should be removed if Radc isn't going to be provided.