Skip to main content
MTomo
Visitor II
October 10, 2018
Question

I am trying to run the S2-lp SDK example project on truestudio but i am running in so many errors? and missing files?

  • October 10, 2018
  • 2 replies
  • 998 views

0690X000006CAEOQA4.pngI am trying to run the S2-lp SDK example project on truestudio but I am running in so many errors. one of them is that the yfuns.h file is not even the directories. 

    This topic has been closed for replies.

    2 replies

    AvaTar
    Senior III
    October 11, 2018

    I don't know this SDK, but it seen your project is not properly set up.

    Have you tried to locate this missing files, and add the appropriate path(es) to te includes ?

    Andrew Neil
    Super User
    October 11, 2018

    Do you mean this: https://www.st.com/en/embedded-software/stsw-s2lp-dk.html ?

    As @Community member​  suggests, the commonest reason for not finding header files (when they do actually exist) is that the Include Paths are not correctly set.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.