Skip to main content
jean-philippe Rey
Associate II
October 10, 2018
Solved

[SOLVED] Problem running STM32CubeProgrammer

  • October 10, 2018
  • 21 replies
  • 12821 views

When running the program STM32CubeProgrammer, an error message appears, saying:

"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". However I have the lastest JAVA SE Run Time installed.

Any idea?

OS:

Windows 10 64-bit

Java:

java version "10.0.1" 2018-04-17

Java(TM) SE Runtime Environment 18.3 (build 10.0.1+10)

Java HotSpot(TM) 64-Bit Server VM 18.3 (build 10.0.1+10, mixed mode)

STM32CubeProgrammer version:

[EDITED]1.2.0

This topic has been closed for replies.
Best answer by Imen.D

Hello,

The issue is fixed with the new STM32CubeProgrammer release V1.2.1.

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html

Kind Regards,

Imen.

21 replies

ST Technical Moderator
October 10, 2018

Hello @jean-philippe Rey​ ,

This is known issue and will be fixed in the coming release of STM32CubeProgrammer.

Please keep an eye out for the next update!

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
LLars.1
Associate
April 18, 2022

As of Apr 18 2022, Version 2.10.0 does not work with Windows 10 (latest) and Java (latest version) Please help

Tesla DeLorean
Guru
April 18, 2022

Please open a NEW thread, this one's 4 years old, and unlikely relevant to current issues.

Is it saying it has missing dependencies, or something entirely different?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jean-philippe Rey
Associate II
October 10, 2018

OK, fine. Any idea when the new version will be released?

Tesla DeLorean
Guru
October 10, 2018

Well V1.0.0 is relatively dated, the current version is V1.2.0

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jean-philippe Rey
Associate II
October 11, 2018

My mistake... I actually installed v1.2.0, which caused the issue

Imen.DBest answer
ST Technical Moderator
November 5, 2018
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
EArthcOnqUEr
Visitor II
April 9, 2019

Hello,

In my case when used release V2.0.0 , this issue was solved after run as administrator.

HMcKi
Associate III
March 6, 2020

Win10 x64 v2.3.0 STM32CubeProgrammer would not work logged in as a non-administrative user, even if you run as administrator.

Updating to v2.4.0 works logged in as a non-administrative user, only if you run as administrator.

Bit dodgy.

JCobu.1
Associate II
March 9, 2020

i'm still not able to make this work. It fails with a message box that says "...API or one of its dependencies is missing. Please try reinstalling your program or check your Java architecture." The message box tool tray icon is from Java, not ST. i have several versions of the JDK installed and the Jave VM. i don't know what else to check.

if anybody from ST is monitoring this, i find this type of software error extremely frustrating.

T_2
Visitor II
September 15, 2019

I bumped into the same issue with v2.1.0.

My setup:

App: STM32CubeProgrammer v2.1.0

App Install path: $HOME/STMicroelectronics/

OS: Fedora-30-workstation 64 bit (Linux 5.2.13-200.fc30.x86_64 #1 SMP Fri Sep 6 14:30:40 UTC 2019 x86_64 GNU/Linux

JAVA runtime: Sun/Oracle [ JRE - **NOT JDK** ]: JRE 1.8 (jre1.8.0_221)

It looks like the java app is unable to locate the libCubeProgrammer_API.so. This is probably happening as I installed it as a standard non-priviledged user. I assume that the installer would normally link those libs from system lib paths when run as admin.

My workaround was to update the LD_LIBRARY_PATH to include the local install directory.

~/.bashrc:

export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:$HOME/STMicroelectronics/STM32Cube/STM32CubeProgrammer/lib/

The app came up okay after that with some null pointer exception logged to console but it seems to work. I haven't tried it with the ST-LINK yet..

Hope this helps.

Bilal.Az
Visitor II
April 22, 2020

Hello, do you mind explaining in a bit more detail how you fixed this issue? I am unable to fix this at my end and would appreciate your help.

JCobu.1
Associate II
February 28, 2020

i've tried installing 2.4.0 on a Win10 machine, both as an administrator and as a user. in both cases the end result is that the startup puts up a message box telling me that the API can't be accessed (the same message as above). i've updated all the Java on this machine and i've successfully run this program on a different machine. if this can't be fixed, can somebody at least explain why one environment works and the other doesn't?

thanks,

Jm

RTN.1
Associate
May 25, 2020

Problem running STM32CubeProgrammer Version 2.4.0 on Mac OS Version 10.10.5.

Keeps throwing error "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program or check your java architecture"

java -version returns

java version "1.8.0_251"

Java(TM) SE Runtime Environment (build 1.8.0_251-b08)

Java HotSpot(TM) 64-Bit Server VM (build 25.251-b08, mixed mode)

Please help. Thanks in advance.

RTN.1
Associate
May 25, 2020

Problem running STM32CubeProgrammer Version 2.4.0 on Mac OS Version 10.10.5.

Keeps throwing error "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program or check your java architecture"

java -version returns

java version "1.8.0_251"

Java(TM) SE Runtime Environment (build 1.8.0_251-b08)

Java HotSpot(TM) 64-Bit Server VM (build 25.251-b08, mixed mode)

Please help. Thanks in advance.