Is it possible to perform asset tracking/indoor localization or to measure RSSI value on a BlueNRG-1/2 board in a bluetooth mesh network ?
I want to track/locate the position of a bluetooth mesh node. I am currently using three BlueNRG-1 based STEVALIDB007v1 boards and an android smartphone to form a bluetooth mesh network in which smartphone reads sensor data from mesh nodes. I did some research and found that RSSI value can be used to estimate the distance between receiver node and a target node. This distance estimate could be used by trilateration method using three nodes (whose positions and distances to target node are already known) to calculate the position of target node.
I would like to ask is it possible to measure RSSI value on BlueNRG-1/2 board in a mesh network ? Or is there any other way to perform asset tracking/indoor localization in a bluetooth mesh network ?