Skip to main content
savatage211
Associate II
October 3, 2018
Solved

STM32L476RG vs STM32L486QX HSE Ready bit

  • October 3, 2018
  • 4 replies
  • 1158 views

Hi,

I am trying to port a software written for STM32L486QX to my STM32L476RG Nucleo board. I have made the board modifications as described in the User manual, except I adjusted the capacitor values for a 19.2 MHz clock. I ran a small program to printf to UART using the HSE clock and it worked, I also measured with a frequency counter and was getting the correct 19.2 MHz within the specified tolerance.

Now when I try to run the code written for the STM32L486QX it gets stuck in the loop where it's waiting for the HSE ready bit. Is there any difference as to the location of this bit for these two CPU's? Or is there something else that obviously jumps out? Thanks in advance for your answers

This topic has been closed for replies.
Best answer by waclawek.jan

> Is there any difference as to the location of this bit for these two CPU's?

Shouldn't be. I'm inclined to accuse your assertion:

> it gets stuck in the loop where it's waiting for the HSE ready bit

How do you know?

Doesn't the original use bypass mode (i.e. an external *oscillator* rather than *crystal*)?

JW

4 replies

waclawek.jan
waclawek.janBest answer
Super User
October 3, 2018

> Is there any difference as to the location of this bit for these two CPU's?

Shouldn't be. I'm inclined to accuse your assertion:

> it gets stuck in the loop where it's waiting for the HSE ready bit

How do you know?

Doesn't the original use bypass mode (i.e. an external *oscillator* rather than *crystal*)?

JW

savatage211
Associate II
October 4, 2018

by stepping through the program execution. Do you know for a fact that there is no such difference between these CPU's?

waclawek.jan
Super User
October 4, 2018

I am not ST.

Have you read out and checked the relevant RCC registers at the place where HSE should be already enabled?

Doesn't the original use bypass mode (i.e. an external *oscillator* rather than *crystal*)?

JW

savatage211
Associate II
October 4, 2018

Closing this. There's no difference in the ready bit or pointers. Traced it to an incorrect debugger setting. Thanks for answering!