Skip to main content
sully
Associate II
September 30, 2018
Question

STM32F412 - Interfacing with 8 PDM microphones

  • September 30, 2018
  • 3 replies
  • 1148 views

I've been reviewing AN5027 (Interfacing PDM digital microphones using STM32) and am a little unclear about a 4x2ch mic configuration using 4 of the SPI/I2S peripherals available on the F412.

Looking at the figure below, could I connect all 4 stereo pairs to the same timer clock output but 4 different I2S_SD lines?

Also, the SPI block shows it connecting to SPIx_MOSI. Shouldn't this be MISO?

Thanks

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    September 30, 2018

    >>Also, the SPI block shows it connecting to SPIx_MOSI. Shouldn't this be MISO?

    Would depend if the STM32 is configured as a Slave

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    sully
    sullyAuthor
    Associate II
    September 30, 2018

    0690X000006C6S3QAK.jpgHmm the image didn't seem to paste properly from my phone. Trying again from my computer. In any case the description for this figure says "the SPI block is configured in master receiver mode".

    waclawek.jan
    Super User
    October 1, 2018

    >>Also, the SPI block shows it connecting to SPIx_MOSI. Shouldn't this be MISO?

    > Would depend if the STM32 is configured as a Slave

    Also, if it would be configured as SPI or I2S - in I2S mode, there's only on data pin, and its direction depends not on whether it's Master or Slave, but whether it's set as Transmitter or Receiver.

    JW