Skip to main content
Emma DULUARD
Visitor II
Sep 28, 2018 1:54 PM UTC
Question

Do you know STM32 Step-by-step ?

Hi all!

We have created for you a new online-education program: STM32 step-by-step.

It is a learning program, part of the STM32 Education initiative, designed for anyone interested in getting started on building projects with the STM32 microcontroller and its powerful ecosystem of development boards and software programming tools.

Our STM32 Step-by-step makes the learning of STM32 ecosystem installation basics easier.

5 tutorials, millions of possibilities : ready to start?

  • Step 1: Tool installation: STM32CubeMX, STM32 TrueSTUDIO, STM32CubeProg, STM32CubeL4
  • Step 2: Blink LED example, pin configuration, start peripherals, Build & generate your projects
  • Step 3: UART and new board introduction, L475 IoT Node Discovery Board, Program and use an RS232 serial link
  • Step 4: Using Sensors on B-L475E-IOT01A (Humidity & temperature / pressure / gyroscope & accelerometer / magnetic)
  • Step 5: Build an IOT system (Data communication via Bluetooth)

Start now and quickly become a professional STM32 developer !

Visit https://www.st.com/stm32stepbystep

Watch our presentation video here: https://www.youtube.com/watch?v=rex-rNSn6XE

    This topic has been closed for replies.

    10 replies

    Ark1
    Associate III
    Sep 29, 2018 5:19 AM UTC

    wonderful initiative:astonished_face: :astonished_face: . it will very useful for developers like me:thumbs_up:

    smaha.0
    Associate II
    Feb 7, 2019 4:50 AM UTC

    thank you Emma..

    i will start know if any dought i will ask.

    thank you very much for giving result Emma

    Sree
    Visitor II
    Jan 7, 2020 5:14 AM UTC

    This was a great initiative! More of this are needed. There are still a lots of developers who are from software background and wanted to learn embedded platforms with ease. This will definitely help the community. Expecting more of such initiatives with working examples and step by step guides. Thanks

    waclawek.jan
    Super User
    Jan 7, 2020 7:31 AM UTC

    Hi @Sree​ ​ ,

    Did you actually try the individual steps with hardware? All 5 steps? Can you please describe some of your findings - were the examples clear, was the PC software easy to find, download and install, did the Android application work as expected, did the examples run out of the box without any problems, do you find them illustrative, would you want to expand on any on the steps further, etc.?

    Thanks,

    JW

    Sree
    Visitor II
    Jan 7, 2020 10:38 AM UTC

    Hi @Community member​ 

    Thanks for taking time to know about the actual or real life experience.

    Luckily, I have purchased the same model hardware i.e. nucleo board even before I came across this step by step tutorial.

    0690X00000BvfMLQAZ.jpg

    The step by step guide is only for Windows machine where as I use a MacOS from which one can understand I have done some ground work to get the things up and running. Looks like the docs are now outdated or the mac environment is different.

    I have followed all the 5 pdfs, reference document links are provided when and where required, for example : USART - a brief explanation pdf was provided. This was helpful to understand what it is exactly.

    Sadly, I was not able to debug as the ST-Link server application is not compatible with mac catalina and I was stuck there. I was able to just execute some example code by generating and pasting the .bin/.hex file on the virtual port of the dev board.

    Although I have imported the code into the STM32CubeIDE (MacOS), I am waiting for a chance to test it on full fledged manner on the dev board.

    There is no official reply from ST team about when the patch for the ST-Link server would be available for Mac OS Catalina.

    Regards,

    Sree

    waclawek.jan
    Super User
    Jan 7, 2020 12:01 PM UTC

    Thanks for sharing your experience, Sree.

    JW

    SGill.1
    Associate
    Feb 11, 2020 11:07 PM UTC

    Will the step-by-step tutorials work with an STM32F401?

    waclawek.jan
    Super User
    Feb 12, 2020 7:37 AM UTC

    I don't know. Step 2 and Step 3 might require to adopt the example for your board, but Step 4 and Step 5 appears to be entirely specific for the 'L4 board so you probably won't be able to use them.

    @Emma DULUARD​  can't these Steps be adopted for other boards?

    JW

    MQi.1
    Senior II
    Feb 14, 2020 3:25 AM UTC

    I have read the tutorials, it is excellent. And, I want to know, when would you make such a tutorial for assembly language programming on STM32 ?

    MQi.1
    Senior II
    Feb 15, 2020 4:26 AM UTC

    I step-by-step by your tutorials, I used NUCLEO-G474RE and CubeIDE. While, when I went down through pdf1, I could not find the file, why?

    "In the window, click Directory and select C:\Users\myname\STM32Cube\Repository\STM32Cube _FW_L4_V1.11.0\Projects\NUCLEOL476RG\Examples_LL\ GPIO\GPIO_InfiniteLedToggling"