2018-09-25 8:01 AM
Hi, this isn't really a question, but I figured I'd share back with the community (and hopefully bring the change back into ST's next release) on the X-CUBE-STL CPU test code.
There are some instances, where the APSR has some bit set in what ARM documents as "reserved" bits. I'm not sure who/what sets them, but occasionally we see some reserved bits set after a firmware update (e.g. DFU).
The result is that the FailSafePOR() hook gets triggered, which in our case performs a NVIC_SystemReset(). After resetting, these reserved bits are cleared and will allow the system to boot properly.
I've added this extra line (with the TLK comment) in the stm32f4xx_STLcpustartGCC.s (v2.1.0) to clear out the bits.
STL_StartUpCPUTest:
MOVS R0, #0x00000000 /* Set Z(ero) Flag */
BNE.W FailSafePOR /* Fails if Z clear */
SUBS R0,#1 /* Set N(egative) Flag */
BPL.W FailSafePOR /* Fails if N clear */
ADDS R0,#2 /* Set C(arry) Flag and do not set Z */
BCC.W FailSafePOR /* Fails if C clear */
MOVS R0, #0x80000000 /* Prepares Overflow test */
ADDS R0, R0, R0 /* Set V(overflow) Flag */
BVC.W FailSafePOR /* Fails if V clear */
MOVS R0, #0xFFFFFFFF /* Prepares Saturation test */
USAT R1,#10,R0 /* Set Q(saturation) Flag */
MRS R0, APSR /* Get Status register */
AND R0, R0, #0xF8000000 /* <--------- TLK: Hack to remove stuff from reserved bits */
CMP R0, #0xB8000000 /* Verifies that N=C=V=Q=1 */
BNE.W FailSafePOR /* Fails if Q+N+C=V clear */Tom
2018-10-08 9:05 AM
Hello,
Thanks for reporting this issue. We need some more details in order to be able to understand it more, and bring the changes.
So, could you please:
Thanks,
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-06-08 10:42 PM
How to apply for X-CUBE-STL package?
2022-11-17 4:49 AM
Hello,
since I'm running in pretty much the same problem I'd like to hook here up.
MRS R0, APSR /* Get Status register */
CMP R0, #0xB8000000 /* Verifies that N=C=V=Q=1 */* @param None
* @retval : None
*/
.section .text.Copy_Handler
.weak Startup_Copy_Handler
.type Startup_Copy_Handler, %function
Startup_Copy_Handler:
/* Copy the data segment initializers from flash to SRAM */
movs r1, #0
b LoopCopyDataInit
CopyDataInit:
ldr r3, =_sidata
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyDataInit:
ldr r0, =_sdata
ldr r3, =_edata
adds r2, r0, r1
cmp r2, r3
bcc CopyDataInit
ldr r2, =_sbss
b LoopFillZerobss
/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2], #4
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
bx lrFinally, APSR is read as 0xB80F 0000 which is the expected value with Reserved bits APSR[19:16] being set.
In the ARM reference manual (DUI553A_cortex_m4_dgug.pdf, see developer.arm.com/documentation/dui0553/latest/) there is a table 2-4 whre these bits are stated as GE[3:0] ' Greater than or equal flags.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.