Question
STM32cubeMX v4.27.0 crashes when "Generate Code" is clicked when creating a new project.
The pc is win10-64bit, I do not have this problem in win7-64. The STM32cubeMX GUI can only be closed in Task Manager where java JRE is reported as "Suspended". Windows java application logs indicate "hangup", timestamped to when I do the clicking. JRE 1.8.181-64bit is installed.
Any advice would be appreciated.