Skip to main content
Jin.Ian
Associate
September 21, 2018
Question

STEVAL-SPIN3202 evaluation board, br2804-1700kv-1 KIT morot and ST Motor Control Workbench V5.2 dosen't work, any idea?

  • September 21, 2018
  • 1 reply
  • 728 views

I generate a STEVAL-SPIN3202 project (Keil MDK) by ST Motor Control Workbench V5.2. But it doesn't work. The motor was BR2804-1700kv-1 sensor less motor from P-NUCLEO-IHM001 KIT.

Motor didn't really spin. I got FOC duration faults when I started motor in Monitor page of Motor Workbench. Communication was OK without problem.

I have other two ST evaluation KIT which are P-NUCLEO-IHM001 and STEVAL-ESC001V1. Both of them work perfectly with ST Motor Control Workbench V5.2 and BR2804-1700kv-1.

My questions are:

  1. Did ST test the STEVAL-SPIN3202 when released ST Motor Control Workbench V5.2? If so, what was my problem. How to make it a work?
  2. Does STEVAL-SPIN3202 really support FOC control?
  3. Does STEVAL-SPIN3202 really support sensor less motor with only one shunt resistor?

Thanks,

Ian

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards