Connecting STM32 NUCLEO board to an external debugger (ARM Keil ULinkPlus)?
Hello,
I'm following this guide (https://mcuoneclipse.com/2015/08/22/debugging-stm32f103rb-nucleo-board-with-with-segger-j-link/)
The board I am using is NUCLEO-L4R5ZI. I've connected the following pins to the 10-pin ARM connector:

I've also tied the VDD_Target/VTref pin to 3.3V.
When I launch Keil uVision5, I go to Project options and select the debugger. I am getting a "RDDI-DAP Error".

Please do not suggest I use the built in ST-LinkV2 debugger as a solution.
Thank you for your help!