Skip to main content
ONDOU
Visitor II
September 18, 2018
Question

Can we create a firmware wich mixes the Lora stack (I-Cube-LRWAN1) and the Sigfox stack (X-Cube-SFOX)

  • September 18, 2018
  • 0 replies
  • 523 views

Hello everybody,

I'm new on this platform.

Currently, I am testing separately, the working of the Lora and Sigfox stacks on the B-L072Z-LRWAN1 evaluation board.

The sample program I use for each stack is the AT Modem. And each stack works very well.

I want now, create a program/firmware wich mixes both stacks. That is, a program that allows with the use of an AT command, to switch from one stack to another. All in one program

So, is there already a program/firmware of this kind?

Thank you in advance for your answers

This topic has been closed for replies.