Question
STM32LO Convert multiple ADCs using DMA
I'm trying to convert 3 ADC channels using DMA. But the variables don't seem to change when I watch them in the debugger. I know the conversion complete callback is executed because I breakpointed it. So this suggests that the DMA transfer is not executing and the buffer is not being filled. I'm using stm32cube to initialize my project so maybe I missed something. I've trimmed the generated code. Thanks.
ADC_HandleTypeDef hadc;
DMA_HandleTypeDef hdma_adc;
uint32_t uwADC8ConvertedValue = 0;
uint32_t uwADC10ConvertedValue = 0;
uint32_t uwADC11ConvertedValue = 0;
uint32_t adcBuffer[3];
/* USER CODE BEGIN 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *AdcHandle) {
uwADC8ConvertedValue = adcBuffer[0];
uwADC10ConvertedValue = adcBuffer[1];
uwADC11ConvertedValue = adcBuffer[2];
}
/* USER CODE END 0 */
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_RTC_Init();
MX_ADC_Init();
MX_USART2_UART_Init();
MX_USART5_UART_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Base_Start_IT(&htim2);
HAL_ADC_Start_IT(&hadc);
HAL_ADC_Start_DMA(&hadc, adcBuffer, 3);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
HAL_UART_Transmit(&huart2, TxBuffer, 15, 5000);
GPIO_PinState userPBstate = OFF;
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin(MODEM_PW_GPIO_Port, MODEM_PW_Pin);
HAL_GPIO_TogglePin(CAM1_LD_GPIO_Port, CAM1_LD_Pin);
HAL_GPIO_TogglePin(CAM1_PW_GPIO_Port, CAM1_PW_Pin);
HAL_Delay(100);
userPBstate = HAL_GPIO_ReadPin(USER_PB_GPIO_Port, USER_PB_Pin);
if (userPBstate == ON) {
HAL_UART_Transmit(&huart2, (uint8_t *)"User button pressed!\n\r", 22, 5000);
}
else {
HAL_UART_Transmit(&huart2, (uint8_t *)"User button NOT pressed!\n\r", 26, 5000);
}
}
/* USER CODE END 3 */
}
/* ADC init function */
static void MX_ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.OversamplingMode = DISABLE;
hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.SamplingTime = ADC_SAMPLETIME_160CYCLES_5;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.DMAContinuousRequests = ENABLE;
hadc.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerFrequencyMode = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_10;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_11;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}