ı try to internal flash codding with STM32L476 ı van erase the banks and pages but HAL_FLASH_Program İS NOT WORKİNG ı get the SR errors(SIZERR,PGSERR) so how can ı fix it
my code is,
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32l4xx_hal.h"
#define FLASH_BSY (1 << 16)
/* Fast programming not used => related errors not used*/
#define FLASH_PGSERR (1 << 7) /* Programming sequence error */
#define FLASH_SIZERR (1 << 6) /* Size error */
#define FLASH_PGAERR (1 << 5) /* Programming alignment error */
#define FLASH_WRPERR (1 << 4) /* Write protection error */
#define FLASH_PROGERR (1 << 3) /* Programming error */
#define FLASH_OPERR (1 << 1) /* Operation error */
#define FLASH_EOP (1 << 0) /* End of operation */
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
uint32_t data;
uint32_t data_1 = 0x11111111;
uint32_t data_2 = 0x22222222;
uint32_t FLASH_ADDRESS;
uint32_t Flash_Data;
uint32_t PageError;
uint32_t i;
HAL_StatusTypeDef status;
uint32_t * adres_data;
uint32_t * deneme_data_adres = (uint32_t *)0x0807F802;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
void Flash_Write(uint32_t FLASH_PROGRAM_ADDRESS, uint32_t Flash_Data);
uint32_t Flash_Read(uint32_t FLASH_PROGRAM_ADDRESS);
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
uint32_t Flash_Read(uint32_t FLASH_ADDRESS)
{
uint32_t Flash_Data;
Flash_Data = *(uint32_t*) FLASH_ADDRESS;
return Flash_Data;
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
*
* @retval None
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
FLASH_EraseInitTypeDef FLASH_EraseInitStructure ;
FLASH_EraseInitStructure.Banks = FLASH_BANK_1;
FLASH_EraseInitStructure.Page = 255;
FLASH_EraseInitStructure.TypeErase =FLASH_TYPEERASE_PAGES;
FLASH_EraseInitStructure.NbPages =1;
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
FLASH_ADDRESS = 0x0807F802;
(*adres_data) = 0x1234;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
//
//Flash_Data = *(uint32_t*)0x0807F802;
//i++;
//Flash_Data = Flash_Read(0x0807F801);
//i++;
//Flash_Data = *(uint32_t*)0x0807F801;
//i++;
//Flash_Data = *(uint32_t*)0x0807F803;
//i++;
//Flash_Data = *(uint32_t*)0x0807F804;
//i++;
//Flash_Data = *(uint32_t*)0x0807F805;
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
status = HAL_FLASH_Unlock();
deneme_data_adres[0] = data_1;
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_PGAERR | FLASH_FLAG_WRPERR | FLASH_FLAG_BSY | FLASH_FLAG_OPTVERR ); // Clear of every FLASH flag
status = HAL_FLASHEx_Erase(&FLASH_EraseInitStructure,&PageError);
status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,0x0807F802,((uint64_t)data_1 << 32) | data_2);
HAL_FLASH_Lock();
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
}
/* USER CODE BEGIN 4 */
void Flash_Write(uint32_t FLASH_PROGRAM_ADDRESS, uint32_t Flash_Data)
{
//uint32_t err;
// HAL_FLASH_Unlock();
//HAL_StatusTypeDef status = HAL_FLASHEx_Erase(&FLASH_EraseInitStructure, &err);
//if(err != 0){}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @param file: The file name as string.
* @param line: The line in file as a number.
* @retval None
*/
void _Error_Handler(char *file, int line)
{
/* USER CODE BEGIN */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/**
* @}
*/
/**
* @}
*/
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/