Skip to main content
Bilge
Associate III
September 10, 2018
Question

ethernet communnication with STM32h7 NUCLEO cubemx and keil

  • September 10, 2018
  • 6 replies
  • 1783 views

I use stm32h7 microcontroller and I want to make ethernet communication cubemx and keil .However I didn't find resources or examples.

This topic has been closed for replies.

6 replies

Khouloud GARSI
ST Employee
September 18, 2018

Hi @Bilge​ ,

I recommend to refer to the example "LwIP_HTTP_Server_Netconn_RTOS" provided under the STM32H7 cube package. It's found under the path below:

STM32Cube\Repository\STM32Cube_FW_H7_V1.3.0\Projects\STM32H743ZI-Nucleo\Applications\LwIP

Also, refer to to the FAQ "Ethernet not working on STM32H7x3":

Link: https://community.st.com/s/article/FAQ-Ethernet-not-working-on-STM32H7x3

Khouloud.

ranran
Senior
December 14, 2018

Hello,

Is there a way to regenerate ico from the ethernet example ?

I find it really difficult to create functional ethernet if I just use stm32cubemx as a starting point.

So, I need to make the example our starting point for the project.

Thanks,

ran

Bilge
BilgeAuthor
Associate III
December 17, 2018

Hi ,

You can make basic configuration on stm32cubemx because some settings come missing and failing to keil from cubemx .I have an application without rtos on my page ,You can look,but there was a packet loses and I din't find any solution .

hkavi.695
Associate II
December 28, 2019

hi @Bilge​ 

I have the same problem, how did you solve your problem?

thanks.

Bilge
BilgeAuthor
Associate III
December 30, 2019

Hi,@hkavi.695​ 

I've struggled stm32h7's ethernet for a long time.There're lots of problem.I got a working ethernet project.The file compiled by cubemx doesn't work so, I shared a running example .This will guide you.

Piranha
Principal III
December 28, 2019

Look at his profile - does it look like he has solved anything? No! Because CubeMX is made by ST's dumb code monkeys and is a swamp, in which you'll stuck and never make network and most of other parts working.

https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32