Question
[Bug] STM32CubeMx fails to update linker scipt when using Makefile as Toolchain
2018-08-21 10:07:21,259 [INFO] ToolchainGenerator:120 - stack trace : java.lang.UnsupportedOperationException: Not supported yet.
at generators.MakefileGenerator.updateHeapAndStack(MakefileGenerator.java:315)
at generators.Generator.generateLinkerFile(Generator.java:715)
at generators.Generator.copyLinkerFile(Generator.java:407)
at convertor.Convertor.generateMakefile(Convertor.java:1436)
at convertor.Convertor.generate(Convertor.java:608)
at convertor.Convertor.convert(Convertor.java:515)
at convertor.Convertor.updateProject(Convertor.java:384)
at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:114)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1780)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:574)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)The even occurs if the stack was not changed, but running java from mingw/git-bash. This might be related to line endings as the linker script has windows line endings. However the ioc is saved with linux line endings when run from mingw/git-bash.