Skip to main content
fm_it
Associate
August 20, 2018
Question

UART Rx interrupt on SPC560D

  • August 20, 2018
  • 1 reply
  • 786 views

SPC5 Studio for SPC560D-DIS board, LINFLEX0 configured as UART, Tx is okay but Rx ISR is not getting called. I am using the auto generated Serial Test application which creates IRQ handlers in "spc5_linflex.c". I have break points set in both Tx and Rx IRQ handlers, only Tx IRQ gets hit. I can see the RX data coming into BDRM buffer and UARTSR DRF (data receive flag) is also set. Please help.

    This topic has been closed for replies.

    1 reply

    procolo
    Visitor II
    August 29, 2018

    Hello,

    are you using spc5studio 5.8.1?

    If not please update your version of SPC5Studio to 5.8.1 and let us know if the problem still exist.

    Regards