DMA transfer error in STM32H7 DCMI
- 5 replies
- 2560 views
Hi all,
I am trying to setup a DCMI example with NUCLEO-H743ZI, the DCMI interrupts work fine, but DMA abrot when transferring the first data and TEIF is set.
The project was setup with CubeMX, and more detail changes is in the git log. I didn't use cache and I've tried to align the buffer, but the problem remains. The Reference manual suggests the following, but I can't figure out what's wrong and how to fix it.
The transfer error interrupt flag (TEIF) is set when:
• A bus error occurs during a MDMA read or a write access
• The address alignment does not correspond to the data size
• The block size is not a multiple of the data size (for source and/or destination): this error is activated on the last transfer and the error address points to the last transfer (which cannot be done)
Any help and suggestions will be greatly appreciated.