Question
When i configure a timer in inverting mode i.e. PWM Generation CH1CH1N than how can i configure the complementary PWM.
I want to generate a pwm in complementary mode such that it has following specs:-
1.Non inverted pwm has to vary from 0 to 90% cycle
2.Inverted pwm reamins in 7% duty cycle
3.Inverted pwm and non inverted pwm does not match at any instant
4.Both wave does not come in a situation that the transition of high will be common