Skip to main content
ASz
Associate
August 8, 2018
Question

STM32F070 ADC Reference voltage problem

  • August 8, 2018
  • 26 replies
  • 6149 views

Hi Everyone!

I have read a lot of topics, articles about the F070 ADC settings, calibration, etc., but I couldn't solve my issue. I'm using ADC with DMA right now, but the problem is the same with the interrupt and the polling method. In my code I'm using 3 channels (2 simple ADCs and the Vref). The result of the Vref channel is about 3.4V but I measure 3.31V with voltmeter (the other channels have this kind of problem too). Calibration is used by every 4th cycle and I have a 100nF capacitor between the Vcc and the GND and input filter as well.

I hope You can help.

Thanks in advance.

Andras

    This topic has been closed for replies.

    26 replies

    T J
    Senior III
    August 9, 2018

    I had the same problem and calibration fixed it with 'F072 and 'F091

    are you driving any heavy loads from another pin ? this can affect the internal rail voltage.

    ASz
    ASzAuthor
    Associate
    August 9, 2018

    No.

    Right now I'm using just the ADC pins, but my final project will use 2 PWMs and UART.

    The calibration helped me a little bit, but I get a 50-70mV difference between the voltmeter's and ADC's value on the ADC pins too (not just Vref).

    T J
    Senior III
    August 10, 2018

    50-70mV you have a problem.

    when did you change the battery in the meter last ? <- this may be your issue, do you have another meter ?

    every bit helps improve the figure...

    a few years ago, I paid a little extra to get a really good Volt Meter. ita an AMProbe 37XR-A

    nothing special, 4 digit and works very well.

    anyhow I am reading 1-2mV difference on the analog input pins and 2-3-4mV on the Vdda calculation.

    it moves around after the re-calibration takes place, cal factor 41-42...

    what sampling speed are you running ?

    the highest few are not good... I use the slowest speed.

    I beef up the Caps all round.. so on Vdda 1u and 0.1u

    lots of 0.1u on the board, if I have a switcher, I use some ferrites and inductors too..

    do you have a switcher power supply ?, this can induce some DC offsets when the noise is rectified in the pin "input stage protection diodes", inside the processor..

    just guessing of course...

    ASz
    ASzAuthor
    Associate
    August 10, 2018

    In my final setup the MCU is working from a battery with a voltage regulator but now I'm using a DC-DC regulator to get 3.3V.

    Now I replaced that regulator with the battery (It is on 3.6V now) and the ADC says its 3.67V. I've made a value correction with a 70mV substraction and it's seems to be right (according to the other values).

    I've tested with another multimeter but it says it's 3.57V so I'm going to get a better multimeter and after that I will check it again.

    T J
    Senior III
    August 10, 2018

    after a power up, you can see the Calibration is off, then after the first cal, all the values seem to settle quite nicely.

    (a 4 digit meter is much better than a 3 1/2 digit... )

    ASz
    ASzAuthor
    Associate
    August 11, 2018

    I have measured with another multimeter but the result is the same :\

    My VCC and VCCA are common (without any cap), could it cause any problem?

    I have included my main.c

    ASz
    ASzAuthor
    Associate
    August 11, 2018

    And this is my ADC settings in the CubeMX

    ASz
    ASzAuthor
    Associate
    August 11, 2018

    ..

    T J
    Senior III
    August 11, 2018

    this is not quite the same ...

    your code is tiny,

    I cant understand why my code is 2000 +lines for a short project,

    yours is under 20...

    void process_ADCcalibration(void) {
    	
     //sprintf(string,"ADC Recal is Progressing\n\r");
     //puts (string);
     
    	
    // check DMA and ADC have stopped;
    /*
    		Calibration software procedure
    		1. Ensure that ADEN=0
    		2. Set ADCAL=1
    		3. Wait until ADCAL=0
    		4. The calibration factor can be read from bits 6:0 of ADC_DR.
    				ADC Calibration code example
    				// (1) Ensure that ADEN = 0 
    				// (2) Clear ADEN 
    				// (3) Launch the calibration by setting ADCAL
    				// (4) Wait until ADCAL=0
    */
    	if((ADC1->CR & ADC_CR_ADEN) != 0)				 // (1) 
     {
     ADC1->CR &= (uint32_t)(~ADC_CR_ADEN); // (2)
     }
     ADC1->CR |= ADC_CR_ADCAL; 							// (3)
     while((ADC1->CR & ADC_CR_ADCAL) != 0) // (4)
     {
     checkBackgroundServices();
     // For robust implementation, add here time-out management 
     }
     ADC_CalibrationFactor = (ADC1->DR); 	//& 0x7F);
     ADChasBeenRecalibrated = true;
     
     HAL_ADC_Start_DMA(&hadc, (uint32_t *)ADC_DMABuffer, ADC_ChannelCount); //from main, adc-start
    		
    } 

    T J
    Senior III
    August 11, 2018

    here is one of my boards setup