Skip to main content
mmell
Associate
August 5, 2018
Question

HI I'm using stm32f103zd and iwm getting after some hours hard fault How can I detect the reason and solve the problem?

  • August 5, 2018
  • 8 replies
  • 2025 views

..

    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    August 5, 2018

    Start by having a proper Hard Fault handler so you can identify the code that is faulting, and the register/stack content.

    Make sure you have a sufficiently large stack, and you understand how much of it is being used.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mmell
    mmellAuthor
    Associate
    August 5, 2018

    HI THANK YOU I'M DOUBLE THE STACK AND IT DID NOT PREVENT FROM HAPPENING -i using the iar workbench so I TRIED TO CATCH WITH IAR

    Can you suggest to me what function to write in hard fault?

    mmell
    mmellAuthor
    Associate
    August 5, 2018

    and it seemed to happen when I'm using the printf or STRCAT function-I not sure

    Tesla DeLorean
    Guru
    August 5, 2018

    For strings make sure you understand the lengths, and that there is NUL termination.

    In Keil we do this, changing startup_stm32xxxx.s to have calling code

    HardFault_Handler\
     PROC
     EXPORT HardFault_Handler
     
     ; Determine correct stack
     
     TST lr, #4
     ITE EQ
     MRSEQ R0, MSP ; Read MSP (Main)
     MRSNE R0, PSP ; Read PSP (Process)
     
     MOV R1, R4
     MOV R2, R5
     MOV R3, R6
     
     EXTERN hard_fault_handler_c
     B hard_fault_handler_c
     ENDP

    //****************************************************************************
     
    void hard_fault_handler_c(unsigned int * hardfault_args, unsigned int r4, unsigned int r5, unsigned int r6)
    {
     printf ("\n[Hard Fault]\n"); // After Joseph Yiu
     
     printf ("r0 = %08X, r1 = %08X, r2 = %08X, r3 = %08X\n",
     hardfault_args[0], hardfault_args[1], hardfault_args[2], hardfault_args[3]);
     printf ("r4 = %08X, r5 = %08X, r6 = %08X, sp = %08X\n",
     r4, r5, r6, (unsigned int)&hardfault_args[8]);
     printf ("r12= %08X, lr = %08X, pc = %08X, psr= %08X\n",
     hardfault_args[4], hardfault_args[5], hardfault_args[6], hardfault_args[7]);
     
     printf ("bfar=%08X, cfsr=%08X, hfsr=%08X, dfsr=%08X, afsr=%08X\n",
     *((volatile unsigned int *)(0xE000ED38)),
     *((volatile unsigned int *)(0xE000ED28)),
     *((volatile unsigned int *)(0xE000ED2C)),
     *((volatile unsigned int *)(0xE000ED30)),
     *((volatile unsigned int *)(0xE000ED3C)) );
     
     while(1);
    }
     
    //****************************************************************************

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mmell
    mmellAuthor
    Associate
    August 5, 2018

    Thank you ,Is there something that is concern on stm32f103zd ?

    Tesla DeLorean
    Guru
    August 5, 2018

    The causes a fairly constrained, and not specific to the STM32F103ZD

    Make sure you don't have any errant pointers, or overflow buffers or local variables. Add sanity checking on pointer.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mmell
    mmellAuthor
    Associate
    August 5, 2018

    Thank for answering me on sunday-What register suppose to show me the problems?

    Tesla DeLorean
    Guru
    August 5, 2018

    You're going to be interested in the PC, the instructions there and immediately before and the registers those instructions are acting upon. They will provide the context of the failure/fault.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..