Skip to main content
DLoha
Visitor II
August 3, 2018
Question

Help needed to select Phase Dimmer Inductor

  • August 3, 2018
  • 0 replies
  • 642 views

Hi,

Greetings!

We are in the process of finalizing 230 Watts load Phase Dimmer Schematic wherein we need some help on below points.

Please find attached copy of Phase Dimmer Schematic for your reference

1. What should be value of “INDUCTOR�? considering LINE SUPPLY to be

  1a. 230VAC to 250VAC, 50-60Hz

  1b. 110VAC to 130VAC, 50-60Hz

2. Make and specifications of Inductor  

  2a. 230VAC to 250VAC, 50-60Hz

  2b. 110VAC to 130VAC, 50-60Hz

3. Are Snubber component values correct?

  3a. 230VAC to 250VAC, 50-60Hz

  3b. 110VAC to 130VAC, 50-60Hz

4. Can we use resettable fuse for short circuit protection? What should be the specifications?   

  4a. 230VAC to 250VAC, 50-60Hz

  4b. 110VAC to 130VAC, 50-60Hz

5. Any protection needed to avoid short circuit failure of Triac?

Regards,

Dinesh

This topic has been closed for replies.